Omron Electroforming

Electroforming is a new technique that has been developed by Omron which enables high‐precision production of extremely small, thin and fine patterned contacts.

What is electroforming?

Electroforming technique overcomes many of the limitations of stamping and pressing.   Not only can smaller, higher quality and higher performance contacts be manufactured, but the tooling process is much simpler and cheaper, reducing investment risk and speeding time to market. Microfabrication technology allows for considerable component design flexibility and is also used to meet more exacting needs for shapes and sizes, since it enables the transfer of a pattern with submicron‐scale (0.0001 mm) surface roughness accuracy. Unlike electroplating, electroforming builds thicker, stronger metal layers which become the actual contact structure.
 
Electroforming is a metal forming process that forms ultra-thin metal components through the electroplating process (Figure 1). The components are produced by developing a layer of metal onto a base form (master). Once the plated layer has been built up to the desired thickness, the newly formed part is stripped off the master substrate. Electroforming enables high-precision production of extremely small, thin and fine patterned parts.

Benefits of EFC

Omron has introduced electroforming technology into the fabrication of the metal parts of connectors, which were previously formed with presswork. This enabled forming narrow parts with a high aspect ratio (ratio of thickness and width). Plates with a width one-third of their thickness have been produced. With traditional pressed contacts it is difficult to allow the plate width to be less than the plate thickness.
 
With electroforming, it is also possible to bend contacts much further. Traditionally, a plate can be bent to a radius of up to twice the plate thickness by dynamic mechanical tooling. Electroforming has achieved a 0.04 mm bend radius by transferring pattern with static chemical processing. This allows for much more freedom in creating round shapes, opening new possibilities in component design.
 
EFC has also allowed micro slits of 35 microns and holes of 50 microns to be created. These were not possible with traditional presswork.
 
With EFC technology, burs on cut edges and warping (undercutting) that are unavoidable with presswork do not occur. A roughness average (Ra) of as little as 0.1 microns can be achieved with EFC, compared to typically 3-10 microns with pressed contacts.
 
In order to reduce the damage to components when attempting to miniaturise them through press work, soft materials with minimal spring strength have to be used. However, electroforming can fabricate complex shapes without risk of processing damage. Therefore, by maximising hardness we can create high spring strength.

Applications of EFC

EFC has already been used to create FPC connectors, battery connectors for smart phones, slit disks for encoders and miniature probes for semiconductor wafers.
In each case, contacts manufactured with EFC bring greater reliability, improved performance and further miniaturisation than was possible with press techniques. For example, in an FPC connector, contact resistance was reduced by 30% from 44 milliohms to 34 milliohms.

Semiconductor probes

EFC contacts are already establishing a lead is probe pins for semiconductors.  Packaging density has been increasing for SMT ICs, LCDs, fine-pitch glass substrates, and other electronic components.  These electronic components have a very large number of pins and electrode pads, and they are laid out very close to each other on a PCB. Inspection of electronic components uses a probe pin. Such high-density devices require inspection of many areas, so multiple probe pins must be placed with a very small spacing between each.  The package unit pitch for recent devices is only 0.4 to 0.5 mm. In a few years, it is expected to be 0.3 mm or less.
 
A probe pin is a slender pin-like part that is used to read electric signals from minute test points when measuring the electrical characteristics of ICs and other electronic parts. It is a key part that is essential in the test sockets that hold the ICs in the inspection devices and the probe cards that are built into the inspection devices.
 
Using EFC an entirely new style of pin has been created, combining four components (upper and lower plungers, spring and conductive path) into one. They have a flat structure which enables placement of pins at any angle, thus making it easier to reduce pitch compared to a conventional cylindrical probe pin. The versatility of electroforming technology enables a single component to incorporate a spring section to provide contact force and durability, and a barrel section that turns on power when it fits the plunger, separate from each other. No electricity flows through the miniaturised spring section, thus solving such problems as excessive temperature rise, the spring section's disconnection, and unstable resistance. Since there is no need for costly investment in press dies and other equipment, as well as the time-consuming die-making process for prototyping and mass production of probe pins, specific demands for customised non-standard specifications can be satisfied speedily.

Omron has produced flat probes of 50 microns thickness, and sockets of 150 micron pitch can be assembled. EFC probes can also be very robust.  (Figure 2) The larger 0.6 mm diameter outer spring type can handle up to 2A. To assemble these tiny contacts, a special air tweezer tool has been created.

The way in which EFC has overcome the limitations of press technology is illustrative. EFC has the potential to transform the connector market (Figure 3), enabling the faster manufacture of prototypes, making smaller production runs economic, and improving the performance of connectors as well as reducing size.
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
This form collects your email address so that our team can communicate with you and provide assistance. Please check our provacy policy to see how we protect and manage the data that you provide. At any moment, you can access, modify or have erased your personal data by sending a request to info-components@eu.omron.com